Add traces at design time (XY Plot)
At design time, you can add a trace with a pair of tags to the XY Plot.
For each trace on an XY Plot object, samples are plotted using horizontal x-axis representing one tag value and a vertical y-axis representing another tag value.
TIP:
To show data from FactoryTalk View SE data logs, make sure the data log models are started. Otherwise, the trend will not show any value of your selected tags.
To trend historical data in
a FactoryTalk Historian
SE server, Asset Framework server, FactoryTalk Historian ME module, or PI Server
, you
need to install FactoryTalk Historian Connectivity
from the FactoryTalk View
installation package on the FactoryTalk View Studio or SE Client computer.All clients must use either the same computer name or the same IP address. If you add or delete a PI server, restart your FactoryTalk View Studio or FactoryTalk View SE Client to take effect.
To add traces to an XY Plot at design time
- On theTracestab ofPropertiesdialog box, click
.
- In theAdd Tracedialog box, click theX Tagbrowse button.
- SelectTag.
- On theTag explorer, expand the tree and navigate to the folder for the data source.
- On theItemspane, select one tag.
- ClickOK.
To add the item as a parameter:- SelectParameter.
- Type a format of#numbersuch as#1.
- ClickOK.
- In theAdd Tracedialog box, click theY Tagbrowse button and repeat the steps in Step 2.
- ClickOK.
Provide Feedback