Set up communications
Use the overview provided below as a guide to the multi-step process needed to set up communications for a network distributed application.
To set up communications for an application:
- Gather information about the network the application will run on and the devices that are connected to it. You need this information to set up the data server that will provide the link to the physical devices on the network.
- Decide which data server you will use for communications between the application and the devices on the network. You can use one of the following:
- FactoryTalk Linxdata server
- OPC data server - data servers that comply with the OPC DA 2.05a, UA 1.02 or 1.03 specifications.
- OPC UA server
- Make sure that the software for the data server you plan to use is installed, and then, using the documentation provided with it, set up the server so that communications between the devices and theFactoryTalk Viewapplication is enabled.
- InFactoryTalk View Studio, add a data server that points to the data server you set up in step 3.
- (optional) If you are going to use HMI tags in the application, open theTagsEditor, and then create tags that haveDeviceas the data source and in theAddressbox specify the OPC item that will provide values for the tag.
- In objects on graphic displays, or anywhere else that tag values are needed, type the HMI tag name.For direct references in devices, type the tag name or address using the syntax for the OPC server, or use theTag Browserto navigate to and select HMI tags or OPC data server tags.TIP:RSLinx Classicis not installed automatically when you installFactoryTalk View SE. For details about installingRSLinx, see theFactoryTalk View SEInstallation Guide, included in theFactoryTalk View SEinstallation package.To useFactoryTalk Linxafter installing it, you have to set it up and add aFactoryTalk Linxdata server to the application. For details on setting upFactoryTalk Linxsee theFactoryTalk LinxHelp.
Provide Feedback