Logic and Control

  • In
    FactoryTalk View Studio
    , the
    Logic and Control
    folder contains editors for setting up alternative ways of manipulating tag data and issuing commands at runtime.
    You can set up:
    • Derived tags
      to derive values from combined tag data.
    • Events
      to trigger actions when specified events occur.
    • Macros
      to issue multiple
      FactoryTalk View SE
      commands in sequence.
    • Client keys
      to assign commands to keyboard keys independent of objects or displays, so that they are always available at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal