Start and stop data logging

DataLogPro starts logging automatically when the HMI server starts, but you can use the context menu or the
DataLogOn
and
DataLogOff
commands to start and stop data logging.
You can run this command from anywhere you can trigger the command, and the command is run on the HMI server side.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal