Undefine

Removes a symbol definition that has been created using the
Define
command.
Syntax
Undefine
<symbol>
where
<symbol>
is the abbreviated command. It cannot contain spaces.
Remarks
This command is run on the
FactoryTalk View SE
Client or
FactoryTalk View Studio
that issued it. It is ignored when it is issued from an HMI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal