FactoryTalk System Status Portal

How do I open the
FactoryTalk
System Status Portal?
  1. In the web browser's address bar, enter one of the following:
    • http://
      <ComputerName>
      /FTSystemStatus
      or
      https://
      <ComputerName>
      /FTSystemStatus
      , where
      ComputerName
      is the
      FactoryTalk
      Directory server computer. For example,
      https://
      <MyFTDPC>
      /FTSystemStatus
      .
    • http://
      <IPAddress>
      /FTSystemStatus
      or
      https://
      <IPAddress>
      /FTSystemStatus
      , where
      IPAddress
      is the IP address of the
      FactoryTalk
      Directory server computer. For example,
      https://
      <192.16.2.1>
      /FTSystemStatus
      .
    TIP:
    If you are signing in from the
    FactoryTalk
    Directory server computer, you can use
    localhost
    to replace
    ComputerName
    or
    IPAddress
    . For example,
    http://localhost/FTSystemStatus
    or
    https://localhost/FTSystemStatus
    .
  2. Press
    Enter
    .
  3. Enter a
    FactoryTalk
    user account with access to the application that you want to view and its password. Select the
    Keep me signed in
    checkbox to stay signed in until you sign out manually or cookies stored by the website in your browser are deleted.
  4. Select
    Sign in
    .
FactoryTalk
System Status Portal provides the system status of network distributed and network station applications without having to install
FactoryTalk View SE
or logging on to the
FactoryTalk Administration Console
or SE Client. This portal is installed with
FactoryTalk Services Platform
by selecting
FactoryTalk
System Status Portal
in customized installation.
The web portal shows the status of the following server types:
  • HMI servers
  • FactoryTalk Alarms and Events
    servers
  • Data servers (
    FactoryTalk Linx
    , OPC UA, and OPC DA servers)
  • FactoryTalk Historian SE and ME servers
  • FactoryTalk AssetCentre servers and agents
The application status will not be influenced by the FactoryTalk Historian SE server, FactoryTalk Historian ME server, and FactoryTalk AssetCentre server and agent, because these servers and agents do not belong to any FactoryTalk application. The icons show the health of each application:
  • system status portal_check means that none of the servers in the application has issues.
  • system status portal_warning means that at least one of the servers in the application has issues.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal