Create a backup
FactoryTalk View SE
Application Manager can back up all contents of the application except the historical data logging in ODBC database or DataLogPro, historical alarm and event logging database, FactoryTalk Historian SE
historical data log. The archive is saved with an .apb extension.
TIP:
You need to manually back up the driver configurations of OPC server, ODBC database, DataLogPro historical records, Alarms and Events historical database, or
FactoryTalk Historian SE
server if you have set up in your application.To create a backup
- InFactoryTalk View SEApplication Manager, select an application type and click theCreate a Backuptab.
- In theChoose Applicationarea, select an application.
- In theReview and Customizearea, specify the following fields if needed:
- Host Machineif redundancy for HMI server is enabled. Select the primary or secondary server to include in the archive.
- Datalogto back up the data log for an HMI server.TIP:Only the internal data logging file sets stored in the default path can be backed up. Otherwise, you need to manually back up the historical data logging files.
- Encrypt the backupto encrypt the file contents.TIP:Remember the password if you select to encrypt the backup. The archive cannot be restored without the correct password.Avoid using the slash symbol (/) in the password because it's not supported in the restoring operation with command.
- In theFinalize and Begin Backuparea, specify the following fields if needed:
- Archive Nameto save the archive with another name.
- Target Folderto save the archive under another folder. The default folder is C:\Users\Public\Documents\RSView Enterprise\SE\Archives.
- ClickBackup.
Provide Feedback