Set up an HMI tag database

An HMI tag database consists of records called
tags
. (A
tag
is similar to a
symbol
in PLC programming terminology.) In the HMI tag database you define the data you want the application to monitor. There is one tag database per HMI server.
To set up a tag database
  • Develop a system of conventions for naming tags.
  • Develop a hierarchy of folders to organize tags into groups.
    For example, a folder that represents a particular area of a plant can contain folders that represent the machines in that area. Each machine folder would contain a group of tags representing the devices being monitored.
  • In the
    Tags
    editor, create the folders and tags that make up the database. To create an HMI tag you specify its name, the type of data it will contain, and its data source. The exact information that is required depends on the tag’s type and data source.
  • In the
    Tags
    editor, set up the alarms for individual tags. You can do this when you add a tag, or you can edit the tag later to add this information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal