Create an HMI tag
The
Tags
editor options listed below are common to all types of tags. To see the additional options for a specific type of tag, go to the help topic for that tag type.To create an HMI tag
- Decide which HMI server you want to create the tag in.
- Open theTagseditor by doing one of the following:
- In theExplorerwindow, double-click theTagsicon in theTagsfolder.
- Right-click theTagstitle and selectOpenfrom the context menu.
- Drag theTagsicon to the workspace.
- To add the tag to a folder, double-click the folder in the folder hierarchy to open it. The folder name appears in theNamebox.
- Click theNewbutton in the form section to clear the form and position the cursor in theNamebox.
- Type the tag name and select its type.
- Enter the additional information required in theTagsection for the type of tag you are creating.
- Choose a data source and enter the information as required for that type of data source.
- ClickAcceptto save the tag to the HMI Tag database.TIP:
- Once you've created a tag, you can't change its type or name by editing them. To rename a tag or change its type, you must duplicate the tag and then supply a new name and type.
- When you enter information in the form, thePrevandNextbuttons change toAcceptandDiscardbuttons. ClickAcceptto save tag information. ClickDiscardto cancel changes to a tag.
- You can also create new tags in the Tag Browser.
Provide Feedback