Grid lines are missing from the trend chart
Problem
A trend chart does not show horizontal or vertical grid lines.
Cause
Several configuration options control the display of grid lines. Set options for horizontal grid lines on the Y-Axis tab. Set options for vertical grid lines on the X-Axis tab.
Possible solutions
On the
Y-Axis
and X-Axis
tabs, verify that:- TheDisplay Grid Linescheck box is selected.
- The number of grid lines is set to a number greater than zero.
- The grid color is not the same color as the chart background. Configure the chart background color on the Display tab.
Provide Feedback