Locate the graphic libraries

To see the location of the graphic libraries (listed under the Libraries icon in the
Explorer
window), in the
Tools
menu, click
Options
and then click the
General
tab.
By default,
FactoryTalk View Studio
Machine Edition stores its library files in
\Users\Public\Public Documents\RSView Enterprise\ME\Libraries
.
To use your own files as libraries instead of the defaults, click the
Browse
button at the right of the window and navigate to the location of the folder containing the files you want to use. The path will appear in the window and the graphic files will appear in the
Libraries
list.
TIP:
To use your own graphic libraries, but still retain the default display libraries such as [DIAGNOSTICS], copy any files you want to include as libraries, from their default location into the folder you are using as the Libraries location.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal