Transfer an application to a MobileView, PanelView Plus 7, PanelView Plus 6, PanelView Plus, PanelView Plus Compact, or PanelView Plus CE terminal
You can use ME Transfer Utility to transfer an application file to a
MobileView
terminal, and to transfer an application or font file to a PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
terminal.To transfer a file to a
MobileView
, PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
terminal- Configure aFactoryTalk Linxdriver on the development computer.
- If you use a serial link or a DH+ network for aPanelView Plus 6,PanelView Plus,PanelView Plus Compact, orPanelView Plus CEterminal, configure the driver on the terminal.
- Use ME Transfer Utility to transfer the file.
Provide Feedback