Select single runtime language
In the
Create Runtime Application Wizard - Select Language
dialog box, choose the language to be included in the runtime application.By default, when the language wizard opens, the current language for the application is selected.
To select a language to be included in the runtime application
- Click on the language to highlight it.
- ClickFinish.
Provide Feedback