Select multiple runtime languages

In the
Create Runtime Application Wizard - Select Languages
dialog box, select the languages to be included in the runtime application.
TIP:
When selecting multiple languages for a runtime application, be sure that you are not running
FactoryTalk View Studio
in the second monitor of a dual monitor system.
Language
check boxes will not accept selections when shown in a secondary monitor.
The runtime language(s) and the initial runtime application language that are selected last time when creating the runtime application are selected by default. If it is the first time you create the runtime application, the current language for the application is selected. The same language appears as the initial runtime language in the box below the language list.
To select the languages to be included and the initial application language for the runtime application
  1. Select the check box for each language to be included in the runtime application.
  2. To change the initial language, from the
    Select the initial runtime application language
    list, select the language.
  3. Click
    Finish
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal