Use the Image Browser to import images

Use the
Image Browser
to import images as needed while setting up a graphic object.
To import an image with the Image Browser
  1. Open the
    Image Browser
    using one of the following methods:
    • In an object’s
      Properties
      dialog box, click the
      Browse
      button next to the
      Image
      box.
      Depending on the type of object, the
      Image
      box could be located on the
      General
      tab,
      Label
      tab, or
      States
      tab.
    • With one or more objects selected, in the
      Property Panel
      , click
      Image
      and then click the
      Browse
      button.
  2. Click
    Add from File
    to open a Windows
    Open
    dialog box.
  3. Select the images to import and click
    OK.
    The dialog box closes and the images appear in the
    Image Browser's Select image
    list.
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal