Import bitmap, JPEG, and PNG images

To use a bitmap, JPEG, or PNG image, import the image and then place it on the display as needed.
FactoryTalk View
installs a set of commonly used PNG images in C:\Users\Public\Documents\RSView Enterprise\Images\Rockwell Library Images. Import them to the
Images
folder to simplify your application development.
To import a bitmap, JPEG, or PNG image
  1. In the
    Graphics
    folder, right-click
    Images
    and then select
    Add Component into Project.
  2. In the
    Files of type
    box, select the type of image to add.
  3. Navigate to the directory where the .bmp, .png, or .jpg file is stored, and then click the file name.
    Shift-click or Ctrl-click to select additional files.
  4. Click
    Open
    to add the selected files to the list in the
    Images
    folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal