Set up electronic signature properties
Use the
E-Signature
tab in the Properties
dialog box to set up electronic signature properties.
TIP:
- The electronic signature function is only supported inFactoryTalk ViewME 8.20 and latter applications.
- If aFactoryTalk ViewME application is imported to aFactoryTalk ViewSE application, the electronic signature properties will not be imported to the SE application.
To set up electronic signature properties
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theE-Signaturetab.
- Specify the electronic signature properties for the object.
Provide Feedback