Set up common properties
Some properties, such as size and position, are common to all graphic objects. Use the
Common
tab in the Properties
dialog box to set up common properties.To set up common properties
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theCommontab.
Provide Feedback