UseVariableLimit
Choose whether the object's upper or lower Ramp value will use a tag or expression value (True), or a constant value (False), at runtime. If a constant value is used, the LimitValue property must be specified. If a tag or expression value is used, the Limit connection must be assigned.
Provide Feedback