LimitValue

If the RampType property is Ramp up, specifies the amount beyond which the button’s value cannot increase.
If the RampType property is Ramp down, specifies the amount beyond which the button’s value cannot decrease.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal