Touch
Specifies whether the object is touch activated. If you select True, the operator can press the object using a touch screen or mouse.
If you select False, the operator must use a keypad or external keyboard to press the object. In this case, use the
Key Assignments
editor to assign a function key to the object.If the object’s Shape property is Circle or Ellipse, the touch area is the object’s bounding box box.
Provide Feedback