Bounding box
The bounding box is a rectangular shape that encloses an object. The application measures in relation to the bounding box to calculate an object’s position, size, caption alignment, image alignment, and touch margins.
For example, an object with an ellipse shape is surrounded by a rectangular bounding box. An image will be positioned on the ellipse by calculating in relation to the edges of the rectangle, not the edges of the ellipse.
Provide Feedback