Top or (GroupTop)
Specifies the number of pixels from the top of the display to position the object or group. You can type a positive or negative number. If you use a negative number, part or all of the object is off screen.
If the object’s Shape property is Circle or Ellipse, the top position applies to the object’s bounding box.
Provide Feedback