Message Handshake connection

Assign a tag or an expression to this connection.
When a message is written to the Message connection, the Message Notification is set to 1.
  • If the Message Handshake connection is not assigned, the Hold Time starts timing. When the Hold Time finishes timing, the Message Notification connection is reset to 0.
  • If the Message Handshake connection is assigned, the Message Notification connection is reset to 0 when the Message Handshake connection changes to a new non-zero value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal