Message connection

This connection allows the message text to be shown elsewhere besides on the alarm graphic display or alarm list.
If you assign this connection and select the
Message to Tag
option for the trigger, when the alarm is triggered, up to 82 characters of the message text is written to this connection. The maximum string length supported by
FactoryTalk View ME
is 82 characters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal