Left or (GroupLeft)

Specifies the number of pixels from the left of the display to position the object or group. You can type a positive or negative number. If you use a negative number, part or all of the object is off screen.
If the object’s Shape property is Circle or Ellipse, the left position applies to the object’s bounding box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal