ImageScaled or St_ImageScaled
Specifies whether to resize the image to fit the object. If the object’s Shape property is Circle or Ellipse, the image is resized to fit in the object’s bounding box, and then clipped to fit the object’s shape.
If this is False, the image is first aligned using the Alignment property, then, if larger than the object, the image is clipped to fit the object.
Provide Feedback