CaptionAlignment or St_CaptionAlignment

Specifies the caption’s position on the object.
If the object’s Shape property is Circle or Ellipse, the position is relative to the object’s bounding box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal