Blink or St_Blink

Specifies whether the object’s background blinks when the object is in this state at runtime. The blink rate is twice per second. If the object has a configured PatternStyle property, the pattern also blinks when the object is in this state.
For objects without states, if Blink is set to True, the object always blinks.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal