PatternStyle or St_PatternStyle

Specifies a pattern for the object or state. The pattern appears on the face of the object.
The pattern does not cover the object’s border, caption, or image. If the object’s BackStyle property is Transparent, the pattern is not visible.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal