Set up general properties for a rounded rectangle or square object

Use the
General
tab of the
Rounded Rectangle Properties
dialog box to set up how a rounded rectangle or square object looks.
To set up general properties for a rounded rectangle or square object
  1. In the
    Graphics Display
    editor, double-click the rounded rectangle or square to open its
    Properties
    dialog box.
  2. On the
    General
    tab, specify the object appearance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal