Set up general properties for a line object

Use the
General
tab of the
Line Properties
dialog box to set up how a line object looks.
To set up general properties for a line object
  1. In the
    Graphics Display
    editor, double-click the line to open its
    Properties
    dialog box.
  2. On the
    General
    tab, specify the object appearance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal