Define custom colors
To define a custom color
- In the color palette, clickOtherto open theColordialog box.
- Select one of theCustom colorsboxes to edit. (This will avoid accidentally editing an existing custom color.)
- In the color refiner box to the right of the basic colors palette, drag the cursor to the area that shows the color you want (in the smallColor/Solidbox), then drag the arrow beside the luminosity bar to adjust the brightness.orType values for Red, Green and Blue, or for Hue, Sat(uration) and Lum(inosity), until you achieve the desired color.
- ClickAdd to Custom Colors.The color is added to the list of custom colors in theColordialog box.TIP:Hue is the position of the color in the color spectrum. Saturation is the purity of the hue, going from gray to the pure color. Luminosity is the brightness of the color, going from black to white.
Provide Feedback