Use the numeric pop-up keypad

To enter numeric values, the operator must open the numeric pop-up keypad by pressing a numeric input enable button or numeric input cursor point object. The keypad can accept up to 17 digits, including the decimal point, leading zero, and minus sign.
When the keypad is open, no other objects in the graphic display can accept input.
To use the numeric pop-up keypad
  1. Press the buttons in the pop-up keypad to enter a value.
  2. Press
    Enter
    Enter symbol.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal