Example: Use a Numeric Input Enable button
In this example, the
Numeric Input Enable
button controls the speed of a conveyor. Pressing this button brings up a keypad or scratchpad (depending on the numeric pop-up setting) that the operator can use to enter the new speed.Create a
Numeric Input Enable
button. Change the maximum value to 100 and set the caption to "Set value."Assign a tag to the Value connection. When the operator presses the button a keypad or scratchpad pops up and the operator can enter a value between the minimum and maximum values. The value entered becomes the value of the Value connection. The data source registers the value change and the conveyor speed changes accordingly.
Provide Feedback