Causes of runtime errors for Enter key handshaking
At runtime, the application logs error messages about Enter key handshaking to diagnostics under these circumstances:
"Enter key handshake time" expires
If the "Enter key handshake time" expires before the Enter Handshake connection resets the Enter connection, the application logs an error.
Enter key handshaking still in effect
If the operator presses the Enter key for an object whose Enter connection has not yet been reset (using a key button or external keyboard or keypad), the application logs an error.
Unassigned connections
If the Value connection is unassigned (or if the object cannot write to the Value connection), the Enter connection is not set to 1 and the application logs an error.
Provide Feedback