Set up general properties for a Numeric Input Enable button

Use the
General
tab of the
Numeric Input Enable Properties
dialog box to set up how a
Numeric Input Enable
button looks.
To set up general options for a Numeric Input Enable button
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify the options.
TIP:
The button does not need to have input focus to invoke a pop-up. It does need to have input focus to ramp the input value.
Once you set up the options on the
General
tab, click the
Label
tab to specify a caption or image for the button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal