Set up general properties for an Information Acknowledge button
Use the
General
tab of the Information Acknowledge Button Properties
dialog box to set up how an Information Acknowledge
button looks.To set up general options for an Information Acknowledge button
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options.
Once you set up the options on the
General
tab, click the Label
tab to specify a caption or image for the button.Provide Feedback