Set up connections for an alarm banner

Use the
Connections
tab of the
Alarm Banner Properties
dialog box to set up connections for an alarm banner.
To set up connections for an alarm banner
  1. In the
    Graphics Display
    editor, double-click the alarm status list to open its
    Properties
    dialog box.
  2. On the
    Connections
    tab, assign a numeric tag to the AlarmIdentifier connection.
TIP:
At runtime, the Alarm Identifier specified on the
Messages
tab of the
Alarm Setup
editor will be written to the numeric tag assigned to the AlarmIdentifier connection only if the
Use Alarm Identifier
check boxes are selected on the
General
tab of the graphic object's
Properties
dialog box and the
Messages
tab of the
Alarm Setup
editor. If the
Alarm Identifier
column is blank on the
Messages
tab of the
Alarm Setup
editor and the
Use Alarm Identifier
check boxes on both tabs are selected, zero will be written to the numeric tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal