Alarm banner
An alarm banner is a list showing only one unacknowledged alarm.
By default, each new unacknowledged alarm overwrites the previous one as long as the object is visible.
If the
Queue new alarms
check box on the Alarm
tab of the Alarm Banner Properties
dialog box is selected, new alarms do not overwrite previous alarms, but are queued in the order they occur. The alarm banner shows the first of the queued unacknowledged alarms. The operator has to acknowledge each alarm individually by the Ack Alarm
button or the Ack All
button to remove it from the queue.Provide Feedback