Set up connections for a String Input Enable button
Use the
Connections
tab of the String Input Enable Properties
dialog box to set up tags and expressions for the button.To set up tags and expressions for a String Input Enable button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to these connections:ValueA write connection. Assign a tag that can support up to 82 characters (bytes). When the operator presses theEnterkey, the application writes the alphanumeric string to the tag's data source.If you do not assign the Value connection, at runtime when the operator presses the button the pop-up does not open.EnterA write connection. Assign a tag to this connection. This connection accepts values of 0 and 1 only. The connection determines how long theEnterkey press is registered. Use this connection for Enter key handshaking.Enter HandshakeA read connection. You can assign a tag or an expression to this connection. This connection resets the Enter connection, using theHandshake reset typeoption specified in theTimingtab. Use this connection forEnterkey handshaking if you want the Enter connection to be reset when a value at the data source changes.If you assign an expression, the application calculates the value of the expression and resets the Enter connection when the expression value meets the conditions of theHandshake reset typeoption.
Provide Feedback