How the String Input Enable button works at runtime

When the operator presses the
String Input Enable
button, the string pop-up keyboard or scratchpad opens. The operator types an alphanumeric string in the pop-up and presses
Enter
. The string is sent to the Value connection at the data source.
If the screen for the computer running the application is too small, the pop-up does not open:
  • If the terminal's resolution is smaller than 236 pixels wide by 208 pixels high, the string pop-up keyboard cannot open.
  • If the terminal's resolution is smaller than 236 pixels wide by 44 pixels high, the string pop-up scratchpad cannot open.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal