Example: Use a String Input Enable button
In this example, the
String Input Enable
button controls the address printed on a label. Pressing this button brings up a keyboard or scratchpad (depending on the string pop-up setting) that the operator can use to enter the new label address.Create a String Input Enable button, change the number of input characters to 22, and set the caption to "Set address."
Assign a string tag to the Value connection. When the operator presses the button, a keyboard or scratchpad pops up and the operator can enter a new address. The value that is entered becomes the value of the Value connection. The data source registers the value change and the label printer now prints this new address.
Provide Feedback