Set up numeric options for a numeric input cursor point

Use the
Numeric
tab of the
Numeric Input Cursor Point Properties
dialog box to set up a numeric pop-up for the object.
To set up a numeric pop-up for the numeric input cursor point
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    Numeric
    tab.
  3. Select a numeric pop-up option:
    • Numeric pop-up keypad
    • Numeric pop-up scratchpad
  4. Specify these properties for the pop-up:
    • Maximum and minimum values
    • Ramp values (if any)
    • Decimal point settings
    • Number of digits (in display settings)
  5. Specify these properties for the shown value:
    • Display settings
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal