Causes of runtime errors for a numeric input cursor point

At runtime, the application logs errors about the cursor point to diagnostics under these circumstances:
Unassigned connections
If the Value connection is not assigned, when the operator activates the numeric input cursor point, the pop-up is not shown and the application logs an error.
Terminal resolution too small
If the computer's resolution is too small to display the numeric pop-up keypad or scratchpad, the pop-up is not shown and the application logs an error.
  • If the terminal's resolution is smaller than 124 pixels wide by 240 pixels high, the numeric pop-up keypad cannot open.
  • If the terminal's resolution is smaller than 124 pixels wide by 68 pixels high, the numeric pop-up scratchpad cannot open.
Ramped value outside minimum and maximum range
If ramping the value either up or down using a key button or a cursor key, causes the value to be greater than the Maximum value or less than the Minimum value (set on the
Numeric
tab):
  • The application logs an error.
  • Nothing is written to the Value connection.
  • The numeric input cursor point will stop ramping until the key button or cursor key has been released and pressed again. Therefore the error will not continue to be logged repeatedly in auto-repeat mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal