Set up general properties for a numeric input cursor point
Use the
General
tab of the Numeric Input Cursor Point Properties
dialog box to set up how a numeric input cursor point looks.To set up general options for the numeric input cursor point
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options.
Provide Feedback