Causes of runtime errors for a Multistate push button

At runtime, the application logs errors about the Multistate push button to diagnostics under these circumstances:
Invalid values
  • If the button’s state value is too large for the data type of the tag assigned to the Value connection, or if the value is outside the assigned tag’s minimum and maximum values, the application does not write the value to the Value connection, the state does not change, and the application logs an error.
    For example, the state value is too large for the tag’s data type if your data source is a
    PLC-5
    , the state value is 2,147,483,647, and the assigned tag is an integer tag using the address N7:0. Integer tags have a range of -32,768 to 32,767.
    If the button is in auto repeat mode when the error occurs, then auto repeat mode ends and the application resets the Auto repeat delay timer.
  • If the Indicator connection value does not match any of the state values for the push button, the button displays the error state.
Unassigned connections
  • If the Value connection is not assigned, the button is shown in its error state. When an operator presses the button, the state does not change and the application logs an error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal