About the Multistate push button's error state

The error state shows at runtime if:
  • The Value connection is unassigned
  • The Value connection value does not match one of the configured state values
  • The Indicator connection value does not match one of the configured state values
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal