Example: Use a Maintained push button

In this example, the
Maintained
push button controls the type of label to print for the bag filler machine. The machine can print labels with metric or imperial weights.
If the operator controls the type of label to print
Create a
Maintained
push button with the caption "Metric selected" for State 0 and "Imperial selected" for State 1. The application monitors the tag you assign to the Value connection to control the label print mode. If the operator presses the button to change the mode, the Value connection value changes, and the machine switches modes.
If a supervisory system controls the type of label to print
If the label print mode can also be set by a supervisory system, the operator must be able to view the application’s local display to see which mode the machine is currently using. In this case, set the
Next state based on
option to Value. This causes the application to read the Value connection and update the button’s state before changing to the next state.
Assign the same tag to the Value connection and the Indicator control. This ensures that the
Maintained
push button always displays the current printing mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal