Set up states for a list indicator

Use the
States
tab to set up how the list indicator's appearance changes to match the value of the Indicator connection.
To set up states for a list indicator object
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    States
    tab.
  3. From the
    Select state
    list, select
    State 0
    .
  4. Specify these properties for State 0:
    • Value
    • Caption
  5. Repeat steps 3 and 4 for each additional state.
Once you set up the properties for one state, you can copy and paste the state’s properties to another state or to all states.
TIP:
To add or remove a state without returning to the
General
tab, click
Insert State
or
Delete State
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal